Post Go back to editing

AD7327 Power-Up Sequence for VDD and VSS

Thread Summary

The user asked about the power-up sequence for VDD and VSS on the AD7327. The final answer states that there is no specific requirement for the power-up sequence, but Schottky diodes should be placed in series with VDD and VSS to prevent damage. This ensures that either VDD-first or VSS-first sequencing is safe.
AI Generated Content
Category: Hardware
Product Number: AD7327

I have a question regarding the power-up sequence for the VDD and VSS supplies of the AD7327.

1. Is there a recommended or required power-up sequence between VDD and VSS?
2. Could powering up VDD before VSS, or VSS before VDD, potentially damage the device?
3. If either sequence could cause damage, which sequence should be followed to ensure reliable operation?

I was unable to find an explicit specification regarding the power-up sequence between VDD and VSS in the datasheet.

Could you please clarify whether the order of powering up VDD and VSS matters, and if either sequence could cause damage to the device?

Thank you for your assistance.

Parents
  • Hi  ,

    There is no documented requirement that VDD must precede VSS or vice versa. However, all supply pins and input pins should remain within the Absolute Maximum Ratings during power-up, power-down, and steady-state operation. The AD7327 datasheet specifically recommends placing Schottky diodes in series with VDD and VSS (as on the evaluation board) to protect the device. With these Schottky diodes in place, either VDD‑first or VSS‑first sequencing will not damage the part because the external diodes prevent current from flowing through internal protection diodes if one rail is present before the other.

    Thanks,
    Francis

  • Hi Francis,

    Thank you for your reply.
    I understand that adding series Schottky diodes to both the VDD and VSS supply lines protects the device regardless of which supply comes up first.

    Your explanation has been very helpful.

    Best regards,

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.