Post Go back to editing

Impact of using internal input buffer

Thread Summary

The user observed a 0.23% gain error with a 1 kΩ series resistor and 100 nF capacitor in unbuffered mode at gain = 1 on the AD7124. Enabling the input buffers is recommended to tolerate higher source impedance and larger RC values without introducing gain error. In buffered mode, the AIN range is limited to AVSS + 100 mV to AVDD - 100 mV.
AI Generated Content
Category: Hardware
Product Number: AD7124
Hello,
I am using the AD7124 with the following configuration:
- Gain = 1
- Unipolar mode
- Internal reference enabled
- Input buffers disabled
To meet EMC requirements, I have placed a 1 kΩ series resistor and a 100 nF capacitor at the ADC input.
During testing, I observed a gain error of approximately 0.23%. When I reduced the series resistance from 1 kΩ to 1 Ω, the error almost disappeared.
The datasheet mentions that RC networks can introduce gain errors when operating in unbuffered mode at gain = 1, but I could not find any quantitative guidance regarding the expected error versus source impedance.
Would enabling the input buffers be the recommended solution in this case?
If the input buffers are enabled, what additional gain error, offset error, or other accuracy degradation should be expected compared to the unbuffered configuration at gain = 1?
Is there any application note or documentation that provides recommendations for maximum source impedance or RC filter values for gain = 1 operation?
Thank you for your support.
 
Best regards,

Parents
  • Hi  ,

    Enabling the input buffers is the recommended solution for your case.

    In unbuffered mode at gain = 1, the ADC input directly drives the modulator sampling capacitor. The datasheet/FAQ explicitly note that with an RC filter in this mode, if the RC time constant is too large, the sampling capacitor cannot fully charge, and gain errors result; therefore, R and C must be limited in unbuffered mode. This matches your observation that reducing the series resistance from 1 kΩ to 1 Ω removed most of the error.

    With the input buffers enabled, the input channel sees the high-impedance buffer input, so significant source impedance and larger RC values can be tolerated without introducing gain error.

    The main trade-off when enabling the buffers at gain = 1 is reduced input voltage headroom: in buffered mode at gain = 1, the absolute AIN range is limited to AVSS + 100 mV to AVDD − 100 mV, whereas in unbuffered mode at gain = 1 it is AVSS − 50 mV to AVDD + 50 mV. The provided sources do not quantify any additional gain or offset error from enabling the buffers beyond this headroom constraint.

    Thanks,
    Francis

Reply
  • Hi  ,

    Enabling the input buffers is the recommended solution for your case.

    In unbuffered mode at gain = 1, the ADC input directly drives the modulator sampling capacitor. The datasheet/FAQ explicitly note that with an RC filter in this mode, if the RC time constant is too large, the sampling capacitor cannot fully charge, and gain errors result; therefore, R and C must be limited in unbuffered mode. This matches your observation that reducing the series resistance from 1 kΩ to 1 Ω removed most of the error.

    With the input buffers enabled, the input channel sees the high-impedance buffer input, so significant source impedance and larger RC values can be tolerated without introducing gain error.

    The main trade-off when enabling the buffers at gain = 1 is reduced input voltage headroom: in buffered mode at gain = 1, the absolute AIN range is limited to AVSS + 100 mV to AVDD − 100 mV, whereas in unbuffered mode at gain = 1 it is AVSS − 50 mV to AVDD + 50 mV. The provided sources do not quantify any additional gain or offset error from enabling the buffers beyond this headroom constraint.

    Thanks,
    Francis

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.