Post Go back to editing

Help with DC2395A-C Evaluation Board and incorrect waveform in PScope

Category: Hardware
Product Number: LTC2325-16

Hello, 

I am using the DC2395A-C and DC890B for a spectroscopy project. I am trying to bring up the hardware by following the instructions in the User Manual, but the output of the ADC that I see in PScope does not match the input signal from a function generator. I have made no modifications to the board or moved any jumpers. I have a 27.5 MHz, 2 Vpp sine wave as the CLK into J9. I am powering with +/- 7V. I am powering the DC890B in CMOS mode. To test the functionality, I am simply driving a 2 Vpp, 20kHz, 0 DC offset sine wave into the top BNC of channel 3. 

The output signal matches the frequency of the input signal, but the amplitude is severely distorted. It is also half-wave rectified. It seems like there is some discrepancy between the board expecting a differential signal versus a single-ended signal. 

I would appreciate any help regarding a possible incorrect hardware/software setup or signal driving. 

Thank you

Images show the input signal displayed on an oscilloscope and the resulting output waveform in PScope. 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.