Post Go back to editing

Is my CCD (and unity gain op-amp) compatible with the AD9826?

Category: Hardware
Product Number: AD9826

Dear All,

I have been working on this design (a CCD with an AFE and an ADC) for a while and I am now at the stage where prototype PCBs have been made (still waiting to receive them), which I will soon begin testing with.

I was going through the datasheets the other day dreading that I might have missed something and then it hit me:

The entire AFE and ADC might not be compatible with the CCD which I am using.

====================================================================

The question:

Please let me know if the AD9826 when used in CDS mode can handle a voltage swing of (a maximum of) 3V from a value (reset level) that is lower than 18V to a value (signal level) that is higher than 12V.

Urgent help is needed and would be appreciated.

====================================================================

Note that the range for Vout for the S9970-1006 is 12V to 18V as stated in the S9970's datasheet.

Note also that the AD9826 can be configured to have a 0-3V or 0-4V input range (In CDS mode the reset level gets clamped to 3V or 4V respectively) as stated in the AD9826's datasheet.

The question is therefore: How high is the reset level (at the output of the unity gain op-amp) allowed to be, before the AD9826's CDSCLK1 pulse occurs (Clamping happens during this pulse).

Please also note the "ABSOLUTE MAXIMUM RATINGS" table for the AD9826.

I have attached a screenshot of the KiCad schematic of the configuration.

Here is a link to the datasheet for the S9970: https://datasheet.sisoog.com/file/7a657573/datasheet/a6d9c62a85df86dbe9061d3c6cf77d5f1a36db54.pdf

The datasheet for the AD9826 is available from analog devices.

Thread Notes

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.