Post Go back to editing

AD7177-2 Can we disable the 50/60Hz filters?

Thread Summary

The user asked about the ability to disable filters in the AD7177-2 ADC. The final answer clarifies that the main Sinc filters (Sinc1, Sinc3, Sinc5) cannot be fully disabled, but the 50/60Hz postfilter can be. Figure 53 in the datasheet shows a choice between Sinc5+Sinc1 and Sinc3, with the 50/60Hz postfilter only operating with Sinc5+Sinc1.

View FAQ
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7177-2

The  AD7177-2 datasheet states that each filter has a registers to enable or disable the various filters:

  SINC1, SINC3, SINC5 and "50Hz and 60Hz Postfilter" 

However Figure 53 implies there is a choice of filter and these cannot be fully disabled.

Hence the subject title.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.