- AVDD and DVDD remain at 3.3 V
- RESET remains pulled high from an always-on 1.8 V rail
- IOVDD drops to 0 V because the system 1.8 V rail is turned off during the ship mode
- No SPI communication is required
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com
Thank you. Any updates on this would be greatly appreciated.
Hi,
No, we would not recommend operating the AD5940 with AVDD and DVDD powered while IOVDD is at 0 V.
This would be a partially powered device condition and would violate the device's operating requirements. In general, powering only some supply domains while leaving others unpowered can create unintended current paths through internal protection structures and digital circuitry.
Regards,
Mark