I'm reading the AD2S1210 datasheet Rev. B, Loss of Signal Detection section, pages 16–17. And I have a question regarding Eqation (5).
Equation (5) states:
- Angular Latency = 2 × Arccos(LOS Threshold / Max Amplitude)
My assumption is this is derived from the monitor signal in Equation (4), which, if one signal is lost and θ = ϕ, simplifies to:
- Monitor = A1 × sin²(θ)
LOS triggers when this hits the LOS threshold:
- A1 × sin²(θ) = LOS Threshold -> θ = Arcsin(sqrt(LOS Threshold / A1)) -> Angular Error = Arccos(sqrt(LOS Threshold / A1))
And doubling that for worst-case latency.
This would mean that a square root is missing in Equation (5). Could you confirm if this is the case or if the angular latency in equation (5) is as intended?
Regards,
David