Post Go back to editing

Power Supply Requirements

Category: Hardware
Product Number: AD7771

Hi,

For AD7771, datasheet recommends two different modes of power supply. One being single ended (3.3V and GND) and the other being dual supply rails (+1.65V and -1.65V). My application requires the dual voltage supply as the the input pins can withstand voltage upto -1.65V. In that case, which power supply should I intend for connecting the rails? Should I go for Negative charge pump based circuit ICs, as the current requirement is less than 100mA or should I follow the transformer based circuit, similar to what has been implemented in the AD7770/AD7771/AD7779 Evaluation board. I have +3.3V and +5V input supply rails available. Can you give me your recommendation on this matter?

Thanks

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.