Post Go back to editing

Get Variation in signal

Category: Hardware
Product Number: Analog Circuit

Our 1mV to 80mV differential signal connect to R104 & R105, Our signal is stable before of R341 & R342, but signal get varied upto 3-5mV after these resistor, IRP_M+ & IRP_M- connect to MCU, We've checked it after removing MCU also, but signal get varied, R326 is connected & REF_CT is 0.632V.

Parents Reply Children
  • A variation of 3–5 mV on a signal that is only 1–80 mV is quite significant. Since you've already removed the MCU and the fluctuation remains, the MCU input is unlikely to be the cause. I would focus on the network around R341, R342, R326, and the REF_CT node. Check whether REF_CT is stable and free of noise, as any disturbance on the 0.632 V reference can couple into the differential signal path. Also verify resistor values, solder joints, leakage paths, and nearby switching or high-current circuits that could be introducing noise. An oscilloscope measurement on both sides of R341/R342 relative to REF_CT may help identify where the variation is being injected.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.