AD2S1210
Production
The AD2S1210 is a complete 10-bit to 16-bit resolution tracking resolver-to-digital converter, integrating an on-board programmable sinusoidal oscillator...
Datasheet
AD2S1210 on Analog.com
Hi,
I have connected all the necessary pins for SPI fron F28379D launchpad to CN0276 using J2.
I was not getting any data, I then connected the /CS to gound by replaciong R57 from 10k to 0ohm.
After instead of 0 and I get 0xFF as read values for all resgister.
I have checked the ground connections and the clock & FSYNC signals they work correct. However I see very low pulses of data on SDI and SDO is always high (with some pulses which dont change beyond threshold voltage).
I am struggling to make this work? Do we need to make any other changes to CN0276 board? do we need to tie VDrive of AD2S1210 to 3.3V of MCU? (if yes, how)
Is there any additinal help material or sample code to try out?
thanks
Sumeet
Hi All, I was able to solve this (I am now able to communicate via SPI from F28379D). Stupid thing was that the SVAL-SDP-CB1Z board cannot be kept connected.
The RD signal is not connectd to the J2 conenctor on CN0276; in this case how do I read the position and velocity in normal mode from AD2S1210 via SPI?
Hi All, I was able to solve this (I am now able to communicate via SPI from F28379D). Stupid thing was that the SVAL-SDP-CB1Z board cannot be kept connected.
The RD signal is not connectd to the J2 conenctor on CN0276; in this case how do I read the position and velocity in normal mode from AD2S1210 via SPI?