AD4080
Recommended for New Designs
The AD4080 is a high-speed, low noise, low distortion, 20-bit, Easy
Drive, successive approximation register (SAR) analog-to-digital
converter (ADC). Maintaining...
Datasheet
AD4080 on Analog.com
C75 is a 1000 pF 1/3 W (wattage makes no sense, but that's what the design files say ツ) making a 1.4 MHz low pass filter on the signal. This seems a bit excessive as smoothing/anti-aliasing for a 40 Msps data converter. Is there any reason not to remove it? What should I watch out for if I do remove it?
Removed C75. Looks good. RMS broadband noise is up from ~8 units to ~9.8, not serious. Who needs simulation when you have hardware? Spectrum is flatter, but I still see the other filter pole's effect. That pole is about where I'd like it, so all is well.
Thank you very much.
Removed C75. Looks good. RMS broadband noise is up from ~8 units to ~9.8, not serious. Who needs simulation when you have hardware? Spectrum is flatter, but I still see the other filter pole's effect. That pole is about where I'd like it, so all is well.
Thank you very much.