Post Go back to editing

No daughter board detected

Thread Summary

The user is unable to detect the EVAL_AD4080ARDZ daughter board on the SDP-K1 using the ACE software. The solution involves ensuring the correct firmware is installed, which can be found in the AD4080 IIO Application documentation. The user should follow the build guide for the firmware if necessary, as the EVAL_AD4080ARDZ does not contain an FPGA.
AI Generated Content
Category: Software
Product Number: EVAL-AD4080ARDZ
Software Version: board.ad4080.1.2026.421203.acezip & ACEInstall_1.30.3369.1491.exe

Hello

I had SDP-K1 and EVAL_AD4080ARDZ in hand now.


I had tried to see same capture on EVAL_AD4080ARDZ users guide Fig11 in the Attched Hardware Panel ...., 

but ' No daughter board detected ' yet.

Would you please adivise?

My procedure is followings,


1) Install ACE Installer software 1.30.3369.1491 in advance

swdownloads.analog.com/.../ACEInstall_1.30.3369.1491.exe


2) Then, click the ' board.ad4080.1.2026.421203.zip' which is downloaded from website in advance.


www.analog.com/.../board.ad4080.1.2026.421203.acezip


3) Set EVAL_AD4080ARDZ on the SDP-K1 , then  Plug in 12V supply. ( SDP-K1 I/O  jumper P14  is 3.3V like as Fig10 on users guide in advance )

4) Plug in USB cable to PC. user

LED DS1 on SDP-K1( orange) is on.  (connected)

LED DS2  on SDP-K1 is on. ( power on)

LED DS1,2,3 on AD40800-ARDZ is on (blue,green, blue)

5) I can see ACE Tinyiiod firmware required pannel, click OK, wait 5-sec,  but nothing changed in the attached Hardware panel. ..... see attached

Q1

Do you think I had to drag & dop any firmware  file into SDP-K1 (D:) manually  when I insert usb cable?? 

If yes, please give me its file.

Q2

Do you think my procedure 2) is wrong?( Not necessary?)   I had tried to follow page 10 of  EVAL- AD4080-ARDZ, but

I coud not follow " ACE slidebar-select packages" ( nothing started.. so I had clicked plug-in ).

Thank you for your support.

Best Regards 

Thread Notes

Parents Reply Children
No Data