Post Go back to editing

EVAL-AD7195ASDZ EXC- is not working properly

Category: Hardware
Product Number: AD7195

Hi,

I am facing following problem: the EXC- does not work with load cell connected to the EVAL-AD7195ASDZ, there is effectively no square wave on this output

I have two such boards and both are having the same failure.

I am connecting scale with HBM load cell (I am having 2 of them and checked every combination).

I am having also some of the old eval boards (AD7195EBZ) and each of them works properly, the excitation behaves as should: I am getting symmetrical square wave with the scale connected

EXC- is red, EXC+ is yellow, load cell connected

EXC- is red, EXC+ is yellow, load cell connected

EXC- is red, EXC+ is yellow, no load cell

EXC- is red, EXC+ is yellow, no load cell

Edit Notes

description fixed
[edited by: mmad at 11:15 AM (GMT -4) on 21 Apr 2026]