Post Go back to editing

Custom firmware upload in EVALAD5940

Category: Software
Product Number: AD5940

Hi, if i upload an example code on EVAL AD5940 from ADI SDK then do i have to do something additional to make the board run by sensor pal gui ? The goal is to make the board run by custom firmware developed for specific applications. So i want to start with ad5940 example firmware and then also make sure that the evaluation board keeps working with sensor pal gui.

Parents
  • Hi,

    Any one can run at a time, not both. If Sensorpal firmware is uploaded, any other custom firmware  present ir in will be erased and overwriten.

    If github/custome firmware is programmed, Sensorpal firmware will be erased and overwritten. 

    Can't run both with one program.

Reply
  • Hi,

    Any one can run at a time, not both. If Sensorpal firmware is uploaded, any other custom firmware  present ir in will be erased and overwriten.

    If github/custome firmware is programmed, Sensorpal firmware will be erased and overwritten. 

    Can't run both with one program.

Children
No Data