Post Go back to editing

Peak Current of Input Pin

Thread Summary

The user inquired about the AD4112's current input pin limits, specifically if the ±50 mA maximum is continuous. The final answer clarifies that ±50 mA is an absolute maximum rating for brief fault tolerance only, not for continuous operation. Continuous current should be within the input current range, which is significantly lower. External current limiting is recommended for sustained or repeated currents near the ±50 mA limit.
AI Generated Content
Category: Hardware
Product Number: AD4112

Hi,

Hi,
For AD4112, as per datasheet, each current input pin can handle max of +-50mA. Is this continuous current?

What is the peak current that each pin can handle and for what duration?

Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.