Hello everyone, i'm currently working with the ad777x-FMCZ devkit, and reading out the channels works fine.
what i'm having trouble with is noticing some weird behaviour on the MISO line, after finishing readiout out all 8 channels.
this is with reading the channels only through SPI. happens when i read the channels in 8 byte frames, or when i try to read all 32 bytes at once.
I might be doing something wrong because for the life of me I cannot understand what is meant in this section of the data sheet.
tbh i think it's quite weirdly written

but in any case, here's what happens on the signal analyzer, first in 8 byte chunk readout.
lines are top to bottom: clock, mosi, miso, /cs,drdy,alert
as you can see, after the last 8 byte chunk is read out, after a while, and after the chip select line is pulled high, we have some weird bit of noise on the line

here is the same thing happening when i try to read out all 32 bytes at once.
i'm sending 0x80 command every 4 bytes, so looks like 0x80, 0x00, 0x00, 0x00, 0x80..... so as to not trigger a reset.
any idea why this might be happening?, the data that i'm getting seems to be good otherwise.