Post Go back to editing

16-bit mode data format issue

Thread Summary

The user observed a 16-sck + 16-sck SPI transaction when reading 16-bit data from the AD4115 ADC, which differs from the datasheet's 8-sck command + 16-sck data. The final answer clarifies that the additional 16 SCLKs are due to the Data+Status option being enabled, which adds 8 SCLKs for the status register. The user confirmed this resolved their issue.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD4115

Hi

In the evaluation software of AD4115, we used the 16-bit mode of AD4115 to read the data from the data_register register of the ADC conversion. We captured the waveform at that time. According to the description in the datasheet, it should be an 8-sck command followed by 16-sck data. However, when we captured it, we found that it was 16-sck + 16-sck (as shown in the following figure). This does not match the description in the datasheet. In our application, which configuration should we follow (datasheet or evaluation software)?

Thanks

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.