Post Go back to editing

daisy chain

Thread Summary

The user seeks to read multiple PT1000 sensors using the AD7793 in a daisy chain configuration but finds that the AD7793 does not support this. The final answer recommends the AD7124-8, which supports multiple RTD sensors, and suggests using the CN-0383 reference design. The user clarifies the need to avoid multiple CS signals and proposes a workaround using a helper circuit and a second CS (CS_CFG) signal to enable daisy chaining.
AI Generated Content
Category: Hardware
Product Number: AD7793

Hi folks!

I intend to read multiple PT1000 sensors. Initially I wanted to use AD7793 in daisy chain operation (with one single CS), but after carefully reading digital interface description, I am pretty sure, AD7793 SPI interface does not support daisy chaining. FOr different reasons, I wanto to avoid multiple CS signals.

Are there any recommendations, maybe another ADC chip?


thanks in advance.
Matthias

  • Hi  ,

    I will contact the product owner and get back to you soon.

    Thanks,
    Francis

  • Hi  ,

    You may want to consider the AD7124-8 Datasheet and Product Info | Analog Devices for your application. It does not support daisy chaining but is able to support multiple RTD sensors to directly interfaced the ADC. We also have a reference design that you may use as a reference in designing your system. CN-0383 (Rev.D)

    Hope this helps.

    Regards,

    JC

  • Hi!

    Thanks for responding. I will use the provided doc to design the analogue stage.


    Some background. I want to create some monitoring devices for (my) home automation. I intend to monitor fill levels of heating oil and rain water storages and probable some more like water grid pressure, temperature and so on. So at different spots, I want to install a display (cpu unit) and attach as much input stages (adc devices) as needed. Each stage allowing one fil sensor (TL136) and on PT1000 to monitor one storage.

    (I will also provide a M-Bus slave connection to remotely readout this data. But this is not related to this topic)


    Unfortunately, The AD7124 is no option as the "problem" is not the number of sensors (alone). My concept will has a cpu device and multpile (1..X) adc devices stacked together as needed. In the software, each device will be pictured by an own instance of a software class. This is why I want to avoid manually adressing like I2C. So SPI daisy chaining would work best. Due to the mentioned issue, I already thought about some kind of helper-circuit to make be able to daisy chain them. 

    My intension is to use a signal to determine, if another adc device is attached. If not, the SPI loop (MOSI/MISO) will automatically be closed:



    And to "addess" only one AD7793, I intend to use a second CS (CS_CFG) signal. This allows me to daisy chain the 74HC595 serial-in-parallel-out shift registers to provide enable signals for only one adc device. When I then use CF_ADC, I can normally talk to the AD7793 as if this ic would be the only one in the SPI loop.






    Thanks & Have a good day

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.