Hello,
I configured my AD7606C-16 in single ended mode. The inputs of the ADC (+ and -) are controlled by an external DAC.
I noticed that the single mode and differential mode return the same value, i only can read the differential mode in any case. When i set the - to 0.5V, and 1V in +, i read 0.5V, in single mode or differential mode.
So whats the difference of those modes? The - is not connected internally to AGND in single ended mode?
So the problem is that i want to correct the common mode error but i can only read the differential mode and not the single-ended mode.