Post Go back to editing

Sin cos resolver

Thread Summary

The user inquires about applying resolver sin cos output directly to an RDC IC with a -2.5V to 2.5V swing. The final answer clarifies that the input voltage should not exceed 4 Vp-p and must not go below 0.2V, suggesting the use of a REFOUT/2 offset voltage to avoid violating absolute maximum ratings. The accompanying answer notes that the maximum amplitude should range from 1.15V to 2V.
AI Generated Content
Category: Hardware
Product Number: AD2S1205

Hi ADI team,

Can I apply resolver sin cos output directly to RDC IC even if resolver output swings -2.5V to 2.5V ? Can I apply negative voltage on pin sinlo of RDC ID? 

As highlighted in this image, is negative resolver output going to shift by Vref/2? Is this what this means? or should I use a clamping circuit to shift negative voltage to min of 1.5V and apply to sinlo pin of RDC?