1) Is it possible to switch the excitation DAC to D5 and D6 at different times to generate two counter electrodes one on CE0 and one on AFE1?
2) Can you share an example code with us to see how the switching between these two main loops should be?
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 14 hours |
DanB mark.ramos Akila RGrau mkhairy |
Awaiting Customer Response |
AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com
1) Is it possible to switch the excitation DAC to D5 and D6 at different times to generate two counter electrodes one on CE0 and one on AFE1?
2) Can you share an example code with us to see how the switching between these two main loops should be?
GenevaC - Moved from How to Use EngineerZone to MEMS Inertial Sensors. Post date updated from Monday, December 8, 2025 9:18 PM UTC to Tuesday, December 9, 2025 3:16 PM UTC to reflect the move.
lallison - Moved from MEMS Inertial Sensors to Precision ADCs. Post date updated from Tuesday, December 9, 2025 3:16 PM UTC to Friday, February 13, 2026 2:55 PM UTC to reflect the move.