Post Go back to editing

EVAL-AD4134FMCZ does not show up in ACE software

Category: Hardware
Product Number: EVAL-AD4134FMCZ, AD4134

Hi! When using the EVAL-AD4134FMCZ  with the SDP-H1, the EVAL-AD4134FMCZ does not get powered and does not show up when following the instructions of the quick start section in the user guide of EVAL-AD4134FMCZ. The SDP-H1 device does show up but without any device attached to it. I have the AD4134 plugins installed as well as all the optional software and drivers when installing the ACE software. The ACE hardware version is 1.30.3369.1491. This setup has also been tested on two separate machines, so I assume that the ACE installation can be ruled out. Any clue what I may be missing to get the EVAL-AD4134FMCZ working with ACE?

Parents Reply Children
  • Hi, I understand as when you initiate ACE, the ACE doesn't read the AD4134. This could be because of EEPROM issue. Do you have provision to probe across C53 on AD4134 EVB. If yes and still ACE not able to read AD4134 this could be due to EEPROM read/write issue. So, by any chance do you happen to unplug the AD4134 EVB from the SDPH1 during power on. As a next step, I recommend testing with an alternate AD4134 evaluation board to rule out hardware-related faults.