Post Go back to editing

How do I benefit from the +/- 40 V SoftSpan mode?

Thread Summary

The user is confused about the ±40 V SoftSpan mode of the AD4858, which requires a supply voltage difference of at least 48 V. The final answer clarifies that the ±40 V range refers to the differential input voltage, not the absolute voltage against ground, and suggests using a ±24 V supply for a ±20 V input range. The AD7606C-18 is recommended as an alternative for a single 5 V supply with ±20 V differential input range.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD4858

I am planning to use the AD4858 in "true bipolar" mode, where all the input signals are relative to a common ground, but can swing both above and below the ground. I am interested in this part primarily because of its "SoftSpan" feature, where I can adjust the input ranges dynamically, per-channel. However, I'm confused about how I can benefit from the highest bipolar SoftSpan mode, which is the +/- 40 V input range.

I am also looking at the TI ADS98xx family (e.g., the ADS9813), which seems to support the equivalent of ADI's SoftSpan. There, I can select a bipolar input range of +/- 12 V, while still powering the chip from a single +5 V analog input. The AD485x seems to work differently. If I am understanding the datasheet correctly, the AD485x needs to be provided with an analog supply voltage that is at least 3.2 V above the highest input voltage. In other words, if I wanted to support an input range of +/- 12 V on the AD485x, I would need to provide >= +15.2 V for VCC (+12 V signal + +3.2 V headroom = +15.2 V) and <= -15.2 V for VEE (-12 V signal - 3.2 V headroom = -15.2 V). First, I just want to double-check whether that is a correct understanding.

Assuming that is correct, I read further that the limits for VCC and VEE are: 10 V <= (VCC - VEE) <= 48 V.

In a "true bipolar" mode, this means that VCC can be no greater than +24 V when VEE is -24 V. That would allow me to handle an input signal of +/- 20.8 V. With this, I would be limited to using the +/- 20 V SoftSpan mode.

How would I possibly be able to use the higher SoftSpan modes of +/- 25 V or +/- 40 V? There is no way that I can power VCC with +40 V and VEE with -40 V, as this would be a difference of 80 V, which is far greater than the maximum allowable supply difference of 48 V. And I would actually need to power VCC and VEE with 3.2 V greater than +/- 40 V.

I feel like I am not understanding something about how this part is supposed to work, because this doesn't make sense to me. How would I benefit from these SoftSpan modes of +/- 25 V and +/- 40 V?

(I understand that if I were measuring a unipolar signal, I could power VCC with, e.g., +44 V and VEE with 0 V, then use the 0-40 V SoftSpan mode. This would still be below the maximum allowable supply difference of 48 V. But there is a SoftSpan mode of +/- 40 V specifically for bipolar inputs, so I am confused about how I would ever be able to make use of that, given the other constraints on powering this chip.)

NOTE: This question would equally apply to all parts in this family, including the AD4855, AD4856, AD4857, etc.

Edit Notes

Changed incorrect note that this contains AI-generated content. It does NOT contain any AI-generated content.
[edited by: CodyGray at 10:24 AM (GMT -5) on 14 Nov 2025]
Parents
  • Hi  ,

    the AD4858 has differential inputs, and the ranges relate to the differential inputs voltages (VINx+ − VINx−), not on the absolute ground related inputs voltages.

    As an Example:

    VIN+ = 20 V (against ground)

    VIN- = -20 V (against ground)

    VDIFF = VIN+ - VIN- = 20 V - (-20 V) = 40 V

    And the other way round:

    VIN+ = -20 V (against ground)

    VIN- = 20 V (against ground)

    VDIFF = VIN+ - VIN- = -20 V - 20 V = -40 V

    And that is how you get a +/-40 V input range.

    Just remember that you have do regard the input voltage as the difference between the +&- inputs pins, not as an absolute voltage of a single pin against ground.

    regards

Reply
  • Hi  ,

    the AD4858 has differential inputs, and the ranges relate to the differential inputs voltages (VINx+ − VINx−), not on the absolute ground related inputs voltages.

    As an Example:

    VIN+ = 20 V (against ground)

    VIN- = -20 V (against ground)

    VDIFF = VIN+ - VIN- = 20 V - (-20 V) = 40 V

    And the other way round:

    VIN+ = -20 V (against ground)

    VIN- = 20 V (against ground)

    VDIFF = VIN+ - VIN- = -20 V - 20 V = -40 V

    And that is how you get a +/-40 V input range.

    Just remember that you have do regard the input voltage as the difference between the +&- inputs pins, not as an absolute voltage of a single pin against ground.

    regards

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.