Post Go back to editing

Design Inquiry

Category: Hardware
Product Number: AD7768

Hi Team,

I'm planning to use the ADC IC AD7768 for my Analog Card. For that i need a differential input amplifier. For me the input to the amplifier is single ended signal coming from the mixer IC AD630ARZ.

Can the amplifier ADA4940-1 works on single ended inputs to differential pair outputs, so that i can convert my single ended signal to diff pair that to be fed into the ADC IC.

For ADA4945-1 I can provide V+ 5V and V- -5V or as recommended in datasheet +7 and -2V.

I'm planning to provide AVDD1 - 5V, AVDD2 - 5V, IOVDD - 1.8V as power supplies for the ADC. For this requirement, i want input range +/-4V for ADC. 

My required input voltage range to the ADC is +/-4V.

The block diagram is shared below.

For the above mentioned supply configuration for ADC and input amplifier does it can provide +/-4V input voltage range for ADC IC and whether ADC can accept those input range values with this supply configuration.

Please provide an update on above query.

Regards,

Abhishek

Parents Reply Children