Post Go back to editing

AD7928: Extend external reference voltage range to 5V.

Thread Summary

The user inquired about the impact on accuracy of the AD7928 when using a 5V reference voltage instead of the specified 2.5V. The final answer confirmed that while the relative accuracy in LSB terms remains the same, the absolute error in volts doubles due to the increased LSB size. The accompanying answer clarified that measuring a 5V signal with either a 2.5V reference and extended range or a 5V reference yields the same absolute error.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7928

Hi, I'm wondering about effect on accuracy on AD7928 when using 5V instead of 2,5V external reference voltage.  Datasheet request is 2.5V +/-1% specified perfomance. REFin to AGND can be set to AVdd. Would it double offset and gain error only or are there other effects to consider like nonlinearity? Thanks

  • Hi,  .

    Your interpretation is correct. Let’s perceive this in terms of LSB size for clarity. With a 2.5 V reference, each LSB corresponds to approximately 0.61 mV. If we increase the reference to 5 V, the LSB doubles to about 1.22 mV. Since most error specifications such as offset, gain, and INL, are expressed in LSBs, their absolute voltage impact also doubles when the LSB size doubles. In other words, the relative accuracy in LSB terms remains the same, but the absolute error in volts scales proportionally with the reference voltage.

    Regards,
    Jo

  • Hi Jo,

    thank you for clarification. In other words measuring a 5V signal with 2,5V reference voltage and extended range or 5V signal with 5V reference provides the same result and absolute error. Best Regards