Post Go back to editing

Do I need to use resistor when grounding unused parallel lines (Dx).

Category: Datasheet/Specs
Product Number: AD7616

Hello,

basically we would like to know if we can dierectly tie the parallel lines (Dx) in serial mode. Datasheet says : "In serial mode, these pins must be tied to DGND." (e.g. for DB0, 1, 2 3). The question raised up, since DBx pins are of DO/DI type is there a possibility that the pins are actively driven even if ADC is configured in Serial Mode (SER/PAR* tied to +3.3V).

Q1:Can we directly tie the pins to DGND without any series resistors?

Q2: If for safe operation resistors are required: what is the proposed value range?

Regards Andreas

  • Hello,

    The recommendation from the datasheet is to tied them directly to DGND. In the eval board we used 100k pull-down resistors, which in the case of selecting SER interface is like a series resistor to ground. If that helps as a reference.

    Regards,

    Lluis.

  • Hello,

    thanks for your feedback. So basically we will use SER mode only for ADC and never plan to use parallel mode. In this case I think we can directly tie to DGND as stated in datasheet and you confirmed. So, can you confirm that the AD7616 device actively never drives DBx pins in SER mode? I guess in Evalboard you have used 100k pull-down resistors since you provide both options SER and parallel mode.

    Regards,

    Andreas

  • Additionally info. We would save 11 resistors per ADC. With an ADC count of 6 these is a total saving of 66 resistors. So, if we can omit those this would be fine due to tight placement needs in our design. In any case safety first: we only omit the series resistors if we are sure that the AD7616 will never drive DBx pins in SER mode.

  • Hi  ,

             In the AD7616, there are pins that have dual function in parallel or in serial modes. There are pins that are used as Data pins in parallel mode, these pins must be connected to DGND. There is also a pin that is used as Data in parallel mode and Dout pin in serial mode like DB11/SDOB. SDOB pin can be in float or unconnected when it is unused. 

    Regards,

    Jonathan