Post Go back to editing

AD7723 Timing Characteristics

Thread Summary

The user inquired about the timing specifications of the AD7723, specifically t6, t7, and t8. The support engineer confirmed that t6 and t7 are 0 to 5 ns, and t8 is 1 clk (max), ensuring that setup/hold times can meet these requirements. The user's application is a communications device with an undecided bandwidth, and they will use the device within the specified time range.
AI Generated Content
Category: Hardware
Product Number: AD7723

Hi,

I am considering the AD7723.

I have a question about the timing specifications.

t6 and t7 are specified as 0 to 5 ns, and the FSI High time of t8 is specified as 1 clk (max).

In order to meet all timing requirements, the setup/hold time must be 0 ns. Are these timing characteristics correct?

Best regards,

Yuya