Post Go back to editing

Reference Gain Correction for the AD4134

Thread Summary

The user inquired about the calculation formula and accuracy of reference gain correction using the REFIN_GAIN_CORR_EN bit on the AD4134. The correction is achieved by multiplying the ADC output code by a stored constant, which is the ratio of the expected digital output (based on the measured voltage on the REFIN pin) to the actual ADC output. This compensates for the voltage drop across the 20 ohm internal resistor. No specific accuracy information was provided.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD4134

Hello.

I have a question regarding reference gain correction using the REFIN_GAIN_CORR_EN bit on the AD4134.

Is there a calculation formula for the reference gain correction?

Also, is there any information available regarding the accuracy of the correction?

Best regards.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.