hi team.
I was designing custom board using AD5940 + MCU.
Since I noticed there is aducm355 which contains MCU itself, I'm moving to aducm355.
As far as I know, In AD5940's BIA example, use CE0 and AIN1 for current, AIN2 and AIN3 for measure voltage.
As ADuCM355 is same AFE, ADuCM355's 4WireZ example also use AIN1~AIN3.
Before making a ADuCM355 based custom board, I would like to use EVAL ADuCM355.
In this development evaluation board, there are RE0, CE0, SE0, DE0 electrodes for sensors connector.
Is it possible to modify the code of 4WireZ and use these electrodes to measure the impedance of 4 electrodes? (CE0 & DE0 for current, RE0 & SE0 for measure voltage)