Post Go back to editing

MAX31855 doesn't detect a short circuit to Vcc

Category: Hardware
Product Number: MAX31855

Hi.

I am designing the hardware with the MAX31855NASA device and I am creating the code to read the temperature it measures with a microcontroller.

I'm running the tests without the thermocouple connected, and it's working correctly, meaning bit 0 (OC Fault) is set to 1.

Now, I've connected the T+ terminal (pin 3) to GND, and all the error bits (from 2 to 0) remain at 0, indicating no errors.

This doesn't seem to make sense.

The full value read is:


0x01501790:

And this is a picture of my hardware:



Any ideas?

Any comments are welcome.

Regards




Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.