Good Morning/Afternoon
I want to avoid to use MAX14906 www.analog.com/.../max14906.html
I need to create a digital output (24V) using AD74412R, Is it possible?
For example using a current output at 4 mA ?
Thanks for your time
Best Regards,
Sergio
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD74412R
Recommended for New Designs
The AD74412R is a quad-channel software configurable input/output solution for building and process control applications. The AD74412R contains functionality...
Datasheet
AD74412R on Analog.com
MAX14906
Production
The MAX14906 is an IEC 61131-2 compliant, high-speed, four-channel industrial digital output, digital input device that can be configured on a per-channel...
Datasheet
MAX14906 on Analog.com
Good Morning/Afternoon
I want to avoid to use MAX14906 www.analog.com/.../max14906.html
I need to create a digital output (24V) using AD74412R, Is it possible?
For example using a current output at 4 mA ?
Thanks for your time
Best Regards,
Sergio
Hi Sergio,
AD74412R was not designed to support DO functions. If you are looking for quad channel alternative, it is possible to use AD74416H, which have integrated DO functionality: AD74416H Datasheet and Product Info | Analog Devices.
If you are looking for workaround with AD74412R without using another chip, I am afraid that simple DO switch will have to be created discretely maybe utilizing 4xGPO on the AD74412R. However, note, that it will require some components to discretely create reliable driver circuit for each channel separately.
Regards,
Arnost
Hi Arnost.
Thanks for the fast answer and the support.
Best regards.
Sergio