Post Go back to editing

seek a replacement for AD7671

Category: Hardware
Product Number: AD7671


I used AD7671 on a circuit 10 years ago, and now I want to upgrade this circuit and seek a replacement for AD7671. I require an increase in the effective value, for example, in the manual of AD7671, the ENOB (effective value) is around 14 between 100kHz and 500Khz. Other parameters are required to remain unchanged, such as packaging and pin definitions, because we do not want to change the program in the FPGA connected to AD7671 in the future.