Post Go back to editing

Decoding the i2c data to voltage

Category: Hardware
Product Number: LTC2497

hi team 

We are using the LTC2497 in single-ended mode, with IN- grounded and a reference voltage (Vref) of 2.5V. Channel 11 is connected to an input voltage of 0.85V. The I2C data read from the LTC2497 is 0xAD47C0, which translates to output_reg[21:6] = 0x00B51F = 46367.

Based on the calculation:
1 * (46367 / 65535) * 0.500 * 2.500 = 0.884V


However, the input voltage remains constant at 0.85V. While other channels are being used to calculate current from other devices, we are using this channel specifically to cross-check the calculations. Despite this, we observe a discrepancy in the calculated result.
Could you confirm if there is an issue with the data decoding or calculations?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.