Post Go back to editing

AD4111 DOUT_RESET

Thread Summary

The user inquired about the practical use cases and implications of setting the DOUT_RESET bit in the AD4111 ADC. The final answer directed the user to a Digital Interface FAQ for detailed information, clarifying that this bit keeps the DOUT/RDY pin in data output mode until CS is brought high. No specific downsides or recommended usage scenarios were provided in the thread.
AI Generated Content
Category: Software
Product Number: AD4111

Hi,

I am exploring the behavior of the DOUT_RESET in AD4111. I understand from the datasheet that enabling this bit causes the DOUT/RDY pin to remain in data output mode until the CS pin is brought high.

However, I would like to gain a deeper understanding of this method and its practical use cases.

  • Are there specific application scenarios or microcontroller interface limitations where setting DOUT_RESET = 1 is strongly recommended or even necessary?
  • Are there any downsides (e.g., performance or power implications) to always keeping DOUT_RESET = 1 regardless of MCU speed (faster MCU)?
  • Is there a recommended approach or guideline for when to enable this bit based on the system design?

Regards,
Lumi

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.