When I was collecting data using the STM32F407 with AD7768, I was able to collect the 3.3V voltage normally. However, while collecting at the ground level, the output from AD7768 fluctuates around 0-4.095V, even when the IN- voltage is greater than the IN+ voltage. Why is this happening?This is the circuit before the input of the AD7768, is it due to the capacitor?