In the EVALUATION BOARD SOFTWARE of AD4115, modify the reference voltage to AVDD-AVSS, select Vin0&Vin1 as differential inputs, input a DC voltage of +10V, and the ADC output voltage is -10V. The input DC voltage is -10V, and the ADC output voltage is +10V. This phenomenon is opposite to that when the reference voltage is External reference and Internal 2.5V reference, with the same input voltage, the voltage polarity output by AD4115 is opposite (that is, when the input is a +10V DC voltage, the ADC output voltage is +10V). Based on this phenomenon, I would like to ask whether it is the chip of AD4115 that shows this phenomenon or if there are problems with our operation during the test?
Thanks,