Post Go back to editing

Synchronise sampling on an interrupt manage by a µC

Thread Summary

The user is trying to synchronize sampling on the AD7779 ADC using an interrupt managed by a microcontroller. The issue is that DRDY pulses do not appear after issuing a sync pulse via the START signal or SPI_SYNC bit. The support engineer suggested checking the configuration of bit 4 in register 0x5F and ensuring a reset pulse is issued after power-up. The user confirmed the ODR is set to 5kHz and will test the SPI_SYNC bit.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD7779

Hello,

Currently, I used an AD7779 with following configuration:

  • Sigma-Delta mode,
  • Sampling each 200µs.

I would like to synchronise sampling on an interrupt manage by my µC as you can show on the following picture:

So is it possible to do this treatment ? If yes, could you tell me how ?

For information, in my application SYNC_OUT and SYNC_IN are linked. I have tried to synchronise sampling using START signal on the interrupt but when I do this, DRDY never come.

Thanks in advance.

Best regards,

Martial

  • Hi  ,

    Do you want the samples to be available every 250 uS or ODR = 4kHz?

    Can you also clarify what "IT Start sampling" means in the figure?

    Whether you apply the sync pulse through SYNC_IN, START, or by writing to SPI_SYNC bit, there should be DRDY pulses after.

    There should be DRDY pulse upon power up. Can you try writing to SPI_SYNC bit?

    Please share the schematic and register settings.

    Thanks,
    Janine

  • Hello Janine,

    Thank you for your reply.

    I set my ODR at 5kHz to have a DRDY pulse each 200µs. I'm not sure to understand the difference between samples available every 250µs and ODR = 4kHz. Could you explain to me ?

    "IT Start sampling" => IT = µC interrrupt and Start sampling = pulse to 0V on START signal

    Here a new figure to explain what I try to do:

    I will try writing to SPI_SYNC bit to see the behavior (maybe Friday, because I can't work on this subject before).

    Below is the schematic:

    I will send you registers values Friday. Following are configuration setting inside C code:

    • PWRMODE = high resolution,
    • Clock prescaler = 1 (DCLK_DIV),
    • ODR = 5kHz,
    • Use external reference.

    Note: if I don't try to command START pin (no synchronization), DRDY signal comes every 200µs.

    Thanks,

    Martial

  • Hello,

    Here you can find all registers value :

    [0]	  unsigned int	0x0000 (Hex)	
    [1]	  unsigned int	0x0000 (Hex)	
    [2]	  unsigned int	0x0000 (Hex)	
    [3]	  unsigned int	0x0000 (Hex)	
    [4]	  unsigned int	0x0000 (Hex)	
    [5]	  unsigned int	0x0000 (Hex)	
    [6]	  unsigned int	0x0000 (Hex)	
    [7]	  unsigned int	0x0000 (Hex)	
    [8]	  unsigned int	0x00FC (Hex)	
    [9]	  unsigned int	0x0000 (Hex)	
    [10]	unsigned int	0x0000 (Hex)
    [11]	unsigned int	0x0000 (Hex)
    [12]	unsigned int	0x0000 (Hex)
    [13]	unsigned int	0x0000 (Hex)
    [14]	unsigned int	0x0000 (Hex)
    [15]	unsigned int	0x0000 (Hex)
    [16]	unsigned int	0x0000 (Hex)
    [17]	unsigned int	0x0064 (Hex)
    [18]	unsigned int	0x0009 (Hex)
    [19]	unsigned int	0x0080 (Hex)
    [20]	unsigned int	0x0020 (Hex)
    [21]	unsigned int	0x0000 (Hex)
    [22]	unsigned int	0x0000 (Hex)
    [23]	unsigned int	0x0000 (Hex)
    [24]	unsigned int	0x0038 (Hex)
    [25]	unsigned int	0x0038 (Hex)
    [26]	unsigned int	0x00C0 (Hex)
    [27]	unsigned int	0x0000 (Hex)
    [28]	unsigned int	0x0000 (Hex)
    [29]	unsigned int	0x0000 (Hex)
    [30]	unsigned int	0x0000 (Hex)
    [31]	unsigned int	0x0055 (Hex)
    [32]	unsigned int	0x0058 (Hex)
    [33]	unsigned int	0x00E5 (Hex)
    [34]	unsigned int	0x0000 (Hex)
    [35]	unsigned int	0x0000 (Hex)
    [36]	unsigned int	0x0000 (Hex)
    [37]	unsigned int	0x0055 (Hex)
    [38]	unsigned int	0x0050 (Hex)
    [39]	unsigned int	0x00C5 (Hex)
    [40]	unsigned int	0x0000 (Hex)
    [41]	unsigned int	0x0000 (Hex)
    [42]	unsigned int	0x0000 (Hex)
    [43]	unsigned int	0x0055 (Hex)
    [44]	unsigned int	0x0057 (Hex)
    [45]	unsigned int	0x0045 (Hex)
    [46]	unsigned int	0x0000 (Hex)
    [47]	unsigned int	0x0000 (Hex)
    [48]	unsigned int	0x0000 (Hex)
    [49]	unsigned int	0x0055 (Hex)
    [50]	unsigned int	0x0053 (Hex)
    [51]	unsigned int	0x00C5 (Hex)
    [52]	unsigned int	0x0000 (Hex)
    [53]	unsigned int	0x0000 (Hex)
    [54]	unsigned int	0x0000 (Hex)
    [55]	unsigned int	0x0055 (Hex)
    [56]	unsigned int	0x0056 (Hex)
    [57]	unsigned int	0x0095 (Hex)
    [58]	unsigned int	0x0000 (Hex)
    [59]	unsigned int	0x0000 (Hex)
    [60]	unsigned int	0x0000 (Hex)
    [61]	unsigned int	0x0055 (Hex)
    [62]	unsigned int	0x0057 (Hex)
    [63]	unsigned int	0x00A5 (Hex)
    [64]	unsigned int	0x0000 (Hex)
    [65]	unsigned int	0x0000 (Hex)
    [66]	unsigned int	0x0000 (Hex)
    [67]	unsigned int	0x0055 (Hex)
    [68]	unsigned int	0x0055 (Hex)
    [69]	unsigned int	0x0055 (Hex)
    [70]	unsigned int	0x0000 (Hex)
    [71]	unsigned int	0x0000 (Hex)
    [72]	unsigned int	0x0000 (Hex)
    [73]	unsigned int	0x0055 (Hex)
    [74]	unsigned int	0x0057 (Hex)
    [75]	unsigned int	0x0095 (Hex)
    [76]	unsigned int	0x0000 (Hex)
    [77]	unsigned int	0x0000 (Hex)
    [78]	unsigned int	0x0000 (Hex)
    [79]	unsigned int	0x0000 (Hex)
    [80]	unsigned int	0x0000 (Hex)
    [81]	unsigned int	0x0000 (Hex)
    [82]	unsigned int	0x0000 (Hex)
    [83]	unsigned int	0x0000 (Hex)
    [84]	unsigned int	0x0000 (Hex)
    [85]	unsigned int	0x0000 (Hex)
    [86]	unsigned int	0x0000 (Hex)
    [87]	unsigned int	0x0000 (Hex)
    [88]	unsigned int	0x00FF (Hex)
    [89]	unsigned int	0x0000 (Hex)
    [90]	unsigned int	0x003F (Hex)
    [91]	unsigned int	0x0000 (Hex)
    [92]	unsigned int	0x003C (Hex)
    [93]	unsigned int	0x0000 (Hex)
    [94]	unsigned int	0x0000 (Hex)
    [95]	unsigned int	0x0010 (Hex)
    [96]	unsigned int	0x0001 (Hex)
    [97]	unsigned int	0x0099 (Hex)
    [98]	unsigned int	0x0000 (Hex)
    [99]	unsigned int	0x0000 (Hex)
    [100]	unsigned int	0x0000 (Hex)
    

    Use SPI_SYNC bit have the same effect describe before : a pulse is generated on SYNC_IN signal and DRDY pulses never appear.

    On the paper, is it possible to do what I have describe before (on figure) ?

    Best regards,

    Martial

  • Hello Janine,

    Do you working on my issue ? If yes, could you give me information ?

    Best regards,

    Martial

  • Hello,

    Is there any progress on the subject?

    Best regards,

    Martial

  • Hi  ,

    Apologies for the delay. The schematic and registers look correct to me except for the bit 4 of register 0x5F. Can you please issue a reset pulse after power-up and check again?

    I would like to clarify, there is DRDY pulse after power-up? But DRDY pulse is gone after issuing a sync pulse using SPI_SYNC register, SYNC_IN pin, or START pin?

    I set my ODR at 5kHz to have a DRDY pulse each 200µs. I'm not sure to understand the difference between samples available every 250µs and ODR = 4kHz. Could you explain to me ?

    From the figure, there is 250uS between DRDY pulses, and I had assumed you wanted to set ODR at 4kHz.

    Thanks,
    Janine

  • Hello,

    Sorry I didn’t see your last response. I don’t understand why you say the register is not set to the correct value, since it is at 0x10, which indicates no error and a complete initialization.

    Thank you for your feedback,

    Martial