Hi,
I am using the EVAL-AD74115H-ARDZ development kit from Analog Devices to implement communication via the Hart protocol with a Siemens SITRANS Probe LU ultrasonic sensor.
I am using the eval-ad74115h-ug-2048 document and the firmware contained in AD74115H_noOS_Drivers-Rel2.0.1 as a reference.
When I run the "CurrentInputExtPowHARTExample" that puts the AD74115H in Duplex mode, everything works correctly, the 74 bytes are sent to the Transmit FIFO and received in the Receive FIFO.
To try to establish Hart communication with the Siemens sensor, I am modifying this same firmware as follows:
HART_PowerUp(TRUE, TRUE, TRUE); //Power up HART + Duplex configuration - for testing purposes ONLY + Enable Frame
to
HART_PowerUp(TRUE, FALSE, TRUE); //Power up HART (use following for end application)
I also added the line below in order to request the PV from the sensor.
WriteToRegister(IDX_CMD_KEY, 0x01); //set command to Read primary Variable
I couldn't find anywhere in the AD74115H firmware or registers where I could set the destination Hart address for the command.
When I run the modified firmware, I see that the EVAL-AD74115H-ARDZ board sends the Hart message on the I/O P and N output, but no response comes from the sensor and the firmware stays in a loop in While(true) "receiving Hart Data".
I suspect it's something related to the destination Hart address for the message, but as I mentioned above, I couldn't find where to set this address in the example firmware. (AD74115H_noOS_Drivers-Rel2.0.1)
I would be very grateful if you could give me some guidance on the steps required for this Hart communication with the sensor.
I simple code exemple would be great.
Thank You

.