Post Go back to editing

floating input in bipolar input mode

Category: Hardware
Product Number: LTC2308

Hello Team,

What would be the output code of LTC2308 when any input channel left open  in bipolar input mode.

What is is input impedance of of LTC2308  can we interface voltage output of sensor directly to the ADC input channel? The sensor minimum load resistance requirement is 250kohm.

Does COM pin require a buffer amplifier to supply Vref/2 voltage in bipolar mode if internal reference 4.096 V is used.?

Thanks and Regards,

Swaminath Katte

Thread Notes