LTC1867
Production
The LTC1863/LTC1867 are pin-compatible, 8-channel 12-/16-bit A/D converters with serial I/O, and an internal reference. The ADCs typically draw only 1...
Datasheet
LTC1867 on Analog.com
LM4040
Production
The LM4040 is a precision two-terminal shunt mode, bandgap voltage reference available in fixed reverse breakdown voltages of 2.048V, 2.500V, 3.000V, 3...
Datasheet
LM4040 on Analog.com
Configuration
* Handwired soldered board.
* ADC input have 49.9R and 1nF cap as in the demo board
* 10K Pot wiper is connected to one input of ADC. other side to GND, 3.3 or LM4040/4.096V reference
* ADC unused inputs connected to GND
* LTC1867 is connected to STM32F401 MCU which has 5V tolerant inputs
* Vref connected with 2.2uF//100nF to ground. RefCOMP with 10uF//100nF to ground
* 5V from external power supply or USB 5V from PC
* Single ended measurement on all 8 channels, each at a time
* All cases use internal reference (no override of Vref)
* Extra care was taken to have a solig ground to to the 1867, LM4040 and inputs
Test #1: Power to LTC1867 via a linear 3.3V regulator from 5V
Vref =2.060V
REFCOMP =3.91V (varies ~ 100mV)
Resolution on all channels is 13 bits or better
3.3V to the pots are used as reference voltage
5V is either from USB or external supply. No difference for resolution.
Using an LM4040 4.096V ext reference to 5V power as the reference to the pots, resolution becomes 11 bits
Test #2: Power to LTC1867 direct from 5V
Vref =2.512V
REFCOMP=3.5V (varies ~ 100mV)
ADC values from pot swings by thousands. Resolution 1 to 2 bits only
When an Input is connected to 5V consistently reads 0xFFFF
All unused input grounds read 0 to 1. Seems SPI data is stable.
5V from PC or 5v from an external power supply makes no difference
Used a multimeter and the 5V Power voltage seems stable within 0.001V (not used scope yet to check noise/ripple)
Adding PI filter on 5V input to LTC1867, (10nF, BLM21 220R@100MHz, 100nf) does not make any difference
Conclusion
3.3 seems to work stable on this circuit, The SPI interface is ruled out to cause strange values
Variance of ADC values over 0x2000 is kind of awkward, likely this is not just noise/ripple.
Question
Why would 5V result in such unstable results (3.3V has pretty good results for an handwired board.
What to further investigate ?
What could be the reason be for REFCOMP to be off in the 5V case ?
As another side question. The datasheet calls out for tantalum bypass capacitors, but the DC806A BOM capacitors listed are all ceramic. Does this mean tantalum is not needed for good performance ?
Reference Buffer Output Pin. Bypass to GND with a 10µF tantalum capacitor in parallel with a
0.1µF ceramic capacitor/ REF (Pin 10): 2.5V Reference Output. This pin can also be used as an external reference buffer input for improved accuracy and drift. Bypass to GND with a 2.2µF tantalum
capacitor in parallel with a 0.1µF ceramic capacitor
The DC0806 BOM uses: 06035A102JAT2A, 0603ZC104MAT2A, 0603ZD105MAT2A, JMK212BJ106MG, LMK212BJ225MG, JMK212BJ475MG.
We procured TAJA225K010RNJ and TAJA225K025RNJ (Mouser states 7 Ohm ESR but it's not mentioned in the datasheet). Would these improve ADC performance ? What ESR is required as there is also TACU series with 5Ohm, F921 with 12 Ohm, TAJR 20 Ohm and TPC1C series with 16Ohm ESR.
Hi, DeBug .
Please see the following insights/questions below:
1) Based on how I understand, you are using internal reference all throughout your tests. Right? What are the values provided like Vref and Refcomp from each tests? Are these your measured values when using 3.3V or 5V to your VDD? And speaking of 3.3V/5V, are these connected to your VDD?
2) Can you provide me a block diagram, or a schematic of your setup/board? This can help me assess your query better regarding the connections of your supplies and your configurations.
3) Nevertheless, may it be a tantalum or a ceramic capacitor, these two components were tested both to contribute to the device to be in its optimal performance. You can use the BOM from its evaluation board as your reference.
Warm regards,
Jo
Hi, DeBug .
Please see the following insights/questions below:
1) Based on how I understand, you are using internal reference all throughout your tests. Right? What are the values provided like Vref and Refcomp from each tests? Are these your measured values when using 3.3V or 5V to your VDD? And speaking of 3.3V/5V, are these connected to your VDD?
2) Can you provide me a block diagram, or a schematic of your setup/board? This can help me assess your query better regarding the connections of your supplies and your configurations.
3) Nevertheless, may it be a tantalum or a ceramic capacitor, these two components were tested both to contribute to the device to be in its optimal performance. You can use the BOM from its evaluation board as your reference.
Warm regards,
Jo
[1] Yes, internal reference. The values of refcomp and vref were provided in the original post above for both 3.3V and 5V Vdd power. These reference/comp pins are not connected to VDD. they are decouple with caps as in DC806A. The VDD (pin 16) is connected to +5 or 3.3V. using 5V values are totally wrong, using 3.3V pretty good.
[2] since it is hand wired, no schematic. it follows the schematic of DC806A without using the external reference. I did test with an LM4040-4.096V but makes no difference.
MCU => SPI => internal vref/refcomp => 8 channels unipolar => cap and serial resistor on inputs => 10K potentiometer on one channel, all others inputs to GND. (via the cap/resistor). 5V from external USB or LM7805 or 3V3 from LM1117-3.3V or via 5V and an RT9059.
[3] Thanks
B.T.W this is not an LTC1876L (which is the 3.3V version)

Schematic as shown. Default: JP8, JP10 short, others open. This is the 5V supply situation and has bad result, Change circuit to 3.3V (JP5 or JP7) result is good. Remove the PI filter has same 5V poor result.
No further progress made. Any suggestions for the schematic as provided above? I'll put a scope on the power to see if there is anything special.
i


Made some measurements. Both with 5V and 3.3V power. The noise on ADC input is about 10mV in both situations. The ADC value is 12 bits with 3V3 power / ADC input and totally inaccurate with 5V. First picture is 5V power supply ans 5V input full scale on ADC input, 2nd picture is 5V AC noise (5V full scale input on ADC is stable at 5V), 3rd is 3V3 AC noise on input with 3V3 full scale Lowering the input voltage input to the ADC does not change the noise level. The reference value for ADC input resistor is taken directly from the power input, which is simply switches from 5V to 3V with a jumper., but it totally changes the measurement accuracy from acceptable accurate to totally inaccurate.