Hello.
Please let me ask new questions about AD7785 here.
For example, with a hysteresis of 017V, Vt(-)=1.83V when Vt(+)=2V, which violates the maximum value of Vt(-), which is 1.7V.
Does this mean that Vt(+)=2V is impossible?
Similarly, with hysteresis 017V, when Vt(-) = 0.8V, Vt(+) = 0.97V, which violates the 1.4V minimum for Vt(+).
Does this mean that Vt(-)=0.8V is also impossible?
In the datasheet, why is the maximum value of Vt(+) 2V and the minimum value of Vt(-) 0.8V?
Best regards