I don't see an IBIS model for the MAX1312. Is there a model for a similar device (same IO design, same process)?
Thanks,
Barry
MAX1312
Production
The MAX1304–MAX1306/MAX1308–MAX1310/MAX1312–MAX1314 12-bit, analog-to-digital converters (ADCs) offer eight, four, or two independent input channels...
Datasheet
MAX1312 on Analog.com
I don't see an IBIS model for the MAX1312. Is there a model for a similar device (same IO design, same process)?
Thanks,
Barry
Hi,
For support regarding this product, please visit one of the technical support pages on our website below for assistance.
Thanks,
Janine