Post Go back to editing

Please tell me about the hysteresis of the AD7785.

Category: Datasheet/Specs
Product Number: AD7785

Hello.

I have a question about AD7785.

i)

Is there an identical AD7785 that has Vt(+)=2V and Vt(-)=0.8V?
Since the time varies depending on where the threshold of the Schmitt trigger input of the AD7785 is located, I would like to know how it may vary in the same device.

ii)

The hysteresis of AD7785 seems to be specified as the width when 1.6V is used as a reference, but in reality, Vt(+) is 1.4V~2.0V and Vt(-) is 0.8V~1.7V, which may be out of the “1.6V±hysteresis” range. I am not sure how to utilize the hysteresis specified in the datasheet in my design.

Best regards.