Post Go back to editing

AD7383-4 connection to QSPI on STM32H753

Category: Hardware
Product Number: AD7383

Hello,

I have a EVAL-AD7383-4FMCZ board and I want to connect this boards to STM32H753 using via QSPI port.

But the problem is, there is no SDI pin on the STM32 QSPI connections, to connect the AD7383 QSPI connection.

What I am thinking at this point is to use only the MOSI output of the STM32's other SPI connection to the SDI port on the AD7383 additionally to QSPI pins.

I wonder, can I complete the missing SDI pin on the STM32 QSPI connection in this way? (Diagram is available in below)

I hope I have asked in a clear way.

Thank you in advance for your valuable help.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.