Post Go back to editing

Using the EVAL-AD7091SDZ Board without the SDZ adapter

Category: Hardware
Product Number: EVAL-AD7091SDZ, AD7091

Hello, currently i am in the process of designing a circuit an need to find an suitable ADC. For that I would like to test the AD7091 ADC using the available EVAL-AD70901 Evaluation Board. The logic which relies on the ADC has already been implemented on a FPGA Eval Board. Now I would like to test this ADC Eval Board in combination with my FPGA Board. I would like to do without the SDZ adapter and the connection to the PC. Is there any way of finding out what the pin assignment looks like on the connection to the adapter board? Based on this I could then connect my FPGA board. Any support or suggestions would be greatly appreciated.

Edit Notes

specified the corresponding EVAL Board
[edited by: MarvinH at 5:30 PM (GMT -5) on 6 Dec 2024]
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.