When powering up the AD7760, the supply pins remain at normal voltage. However, when I tried to write a program, the AD7760's Vdrive from the DVDD would change from 2.5V to 2.8V and the AD7760 would not work. I checked my PCB and found that the coupled ground of PIN12 is not connected back to PIN9 but directly to system ground as shown below. Could this be the cause of the AD7760 not working.