Post Go back to editing

when it is used single-ended input , input voltage range (0.37 gain)

Category: Datasheet/Specs
Product Number: ADAQ23876

 . ADAQ23876 DATASHEET . figure 76 ADAQ23876 Single-Ended input Configuration with Gain = 0.37 

In that picture, the input range seems to be -10V to 10V
But I think -5V to +5V is correct.
Because at 0.37gain, +5.534v is the maximum value at 2.048V, and -5.53514v is the minimum value at -2.048V.
Also, V- is ground.
V+ V- should have an output of -5V to 5V,
I was wondering if I missed something.

Thread Notes

Parents
  • Hello, 

    As stated in the Voltage Reference Input section (Page 30) of the datasheet, the ADAQ23876 offers three voltage reference options: 

    1. Internal 2.048V reference with Internal Reference Buffer (G =2)
    2. External 2.048V Reference with Internal Reference Buffer (G =2)
    3. External 4.096V Reference with External Reference Buffer (Internal Reference Buffer Overdriven)

    When using an internal or external 2.048V reference, an internal buffer gains (G=2, see Figure 1) this reference voltage by 2× to 4.096V at the REFBUF pin, so in any case, the voltage difference between REFBUF and GND determines the full-scale input range (i.e. +/-4.096 V) of ADC inside the ADAQ23876, so the typical ±10 V (SE or differential) input range for G =0.37 and for all other gain/input range configurations presented in Table 8 as well as the Applications diagrams (Figure 71-80) in the datasheet are correct.

    Hope that helps!

    It would be great If you can share any detail about your end application use case.

    Thanks,
    Maithil

Reply
  • Hello, 

    As stated in the Voltage Reference Input section (Page 30) of the datasheet, the ADAQ23876 offers three voltage reference options: 

    1. Internal 2.048V reference with Internal Reference Buffer (G =2)
    2. External 2.048V Reference with Internal Reference Buffer (G =2)
    3. External 4.096V Reference with External Reference Buffer (Internal Reference Buffer Overdriven)

    When using an internal or external 2.048V reference, an internal buffer gains (G=2, see Figure 1) this reference voltage by 2× to 4.096V at the REFBUF pin, so in any case, the voltage difference between REFBUF and GND determines the full-scale input range (i.e. +/-4.096 V) of ADC inside the ADAQ23876, so the typical ±10 V (SE or differential) input range for G =0.37 and for all other gain/input range configurations presented in Table 8 as well as the Applications diagrams (Figure 71-80) in the datasheet are correct.

    Hope that helps!

    It would be great If you can share any detail about your end application use case.

    Thanks,
    Maithil

Children