Hi, I am getting this CV for the parameters mentioned in another screenshot. I am not able to correlate with the potential I have entered and the I-V CV curve I am getting. Please help me. Thank you.
ADUCM355
Recommended for New Designs
The ADuCM355 is an on-chip system that controls and measures electrochemical sensors and biosensors. The ADuCM355 is an ultralow power, mixed-signal microcontroller...
Datasheet
ADUCM355 on Analog.com
AD5940
Recommended for New Designs
The AD5940 and AD5941 are high precision, low power analog front ends (AFEs) designed for portable applications that require high precision, electrochemical...
Datasheet
AD5940 on Analog.com


Hi, I am getting this CV for the parameters mentioned in another screenshot. I am not able to correlate with the potential I have entered and the I-V CV curve I am getting. Please help me. Thank you.
lallison - Moved from StudentZone (Analog Dialogue) to Precision ADCs. Post date updated from Thursday, October 17, 2024 7:40 PM UTC to Tuesday, June 24, 2025 9:10 PM UTC to reflect the move.
lallison - Moved from StudentZone (Analog Dialogue) to Precision ADCs. Post date updated from Tuesday, June 24, 2025 9:10 PM UTC to Tuesday, June 24, 2025 9:10 PM UTC to reflect the move.
Hi,
May I know if your are using the "AD5940_Ramp" code available in Github?
For above configuration,
RE0 and SE0 voltages are as shown below:
Yellow: SE0
Red: RE0

VRE0 - VSE0 varies from -900mV to 300mV.
VSE0 is fixed at 1.3V.
Corresponding current vs stimulus data for a is below:
Stimulus (mV) Current (mA) -899.8779297 0.764910758 -895.5800171 0.199679121 -891.2821045 0.20598951 -886.9841309 0.217708841 -882.6861572 0.22582221 -878.3883057 0.232583359 -874.0903931 0.237541512 -869.7924805 0.241147473 -865.4945068 0.242499694 -861.1966553 0.243851915 -856.8986816 0.247908592 -852.600769 0.247457862 -848.3028564 0.250162333 -844.0048828 0.248359352 -839.7069702 0.250162333 -835.4090576 0.250162333 -831.111145 0.253317535 -826.8132324 0.250162333 -822.5152588 0.251063824 -818.2173462 0.252866775 -813.9194336 0.250162333 -809.621521 0.252866775 -805.3236084 0.251063824 -801.0256348 0.252866775 -796.7277222 0.251965284 -792.4298096 0.251965284 -788.131897 0.251965284 -783.8339844 0.251514554 -779.5360107 0.251965284 -775.2380981 0.251063824 -770.9401855 0.251514554 -766.6422729 0.251063824 -762.3443604 0.252866775 -758.0463867 0.251063824 -753.7484741 0.252866775 -749.4505615 0.251965284 -745.1526489 0.254219025 -740.8547363 0.251965284 -736.5567627 0.252416044 -732.2589111 0.252416044 -727.9609375 0.251063824 -723.6630249 0.251965284 -719.3651123 0.251063824 -715.0671387 0.250162333 -710.7692871 0.251965284 -706.4713135 0.250162333 -702.1734009 0.252866775 -697.8754883 0.251063824 -693.5775146 0.252416044 -689.2796631 0.250613064 -684.9816895 0.252866775 -680.6837769 0.251514554 -676.3858643 0.251063824 -672.0879517 0.253317535 -667.7900391 0.251514554 -663.4920654 0.251965284 -659.1941528 0.251063824 -654.8962402 0.251063824 -650.5983276 0.251965284 -646.300415 0.250613064 -642.0024414 0.252866775 -637.7045288 0.253317535 -633.4066162 0.251965284 -629.1086426 0.250613064 -624.810791 0.252416044 -620.5128174 0.252416044 -616.2149048 0.252866775 -611.9169922 0.251965284 -607.6190186 0.251063824 -603.321167 0.252866775 -599.0231934 0.250613064 -594.7252197 0.251063824 -590.4273682 0.252866775 -586.1293945 0.251514554 -581.831543 0.252416044 -577.5335693 0.251965284 -573.2357178 0.251965284 -568.9377441 0.251063824 -564.6398315 0.251063824 -560.3419189 0.252866775 -556.0439453 0.251063824 -551.7460327 0.253317535 -547.4481201 0.253768265 -543.1502075 0.251965284 -538.8522949 0.251965284 -534.5543213 0.252866775 -530.2564087 0.251965284 -525.9584961 0.252416044 -521.6605835 0.251965284 -517.3626709 0.251514554 -513.0646973 0.253317535 -508.7667847 0.251514554 -504.4688721 0.252866775 -500.1709595 0.252416044 -495.8730164 0.251965284 -491.5751038 0.252416044 -487.2771606 0.251514554 -482.979248 0.251063824 -478.6813354 0.251965284 -474.3833923 0.251514554 -470.0854797 0.252416044 -465.7875671 0.253768265 -461.489624 0.251965284 -457.1917114 0.251063824 -452.8937683 0.251965284 -448.5958557 0.251965284 -444.2979431 0.252866775 -440 0.251514554 -435.7020874 0.253768265 -431.4041443 0.252416044 -427.1062317 0.251965284 -422.8083191 0.251965284 -418.510376 0.251965284 -414.2124634 0.251965284 -409.9145203 0.252866775 -405.6166077 0.253317535 -401.3186951 0.251965284 -397.020752 0.251965284 -392.7228394 0.252416044 -388.4249268 0.252416044 -384.1270142 0.253317535 -379.8290405 0.251965284 -375.5311279 0.252866775 -371.2332153 0.251965284 -366.9353027 0.251063824 -362.6373901 0.255120486 -358.3394165 0.252866775 -354.0415039 0.252866775 -349.7435913 0.251514554 -345.4456787 0.251965284 -341.1477661 0.253768265 -336.8497925 0.252866775 -332.5518799 0.253317535 -328.2539673 0.251965284 -323.9560547 0.251514554 -319.6581421 0.251063824 -315.3601685 0.253317535 -311.0622559 0.251965284 -306.7643433 0.252416044 -302.4664307 0.251965284 -298.1685181 0.252866775 -293.8705444 0.252416044 -289.5726318 0.253768265 -285.2747192 0.252416044 -280.9768066 0.253317535 -276.678894 0.253768265 -272.3809204 0.252866775 -268.0830078 0.251965284 -263.7850952 0.249711588 -259.4871826 0.253768265 -255.18927 0.251063824 -250.8913574 0.251965284 -246.5933838 0.252866775 -242.2954712 0.252416044 -237.9975586 0.250613064 -233.699646 0.252416044 -229.4017334 0.251965284 -225.1037598 0.252866775 -220.8058472 0.252416044 -216.5079346 0.252866775 -212.210022 0.252866775 -207.9121094 0.251965284 -203.6141357 0.255120486 -199.3162231 0.252866775 -195.0183105 0.252416044 -190.7203979 0.253317535 -186.4224854 0.252866775 -182.1245117 0.253317535 -177.8265991 0.252866775 -173.5286865 0.252416044 -169.2307739 0.253317535 -164.3955688 0.251063824 -160.0976563 0.251063824 -155.7997437 0.253768265 -151.5018311 0.252866775 -147.2039185 0.252866775 -142.9059448 0.252866775 -138.6080322 0.251965284 -134.3101196 0.252866775 -130.012207 0.252866775 -125.7142944 0.252866775 -121.4163208 0.252416044 -117.1184082 0.253317535 -112.8204956 0.251965284 -108.522583 0.251514554 -104.2246704 0.253317535 -99.92675781 0.252866775 -95.62878418 0.250613064 -91.33087158 0.252866775 -87.03295898 0.252866775 -82.73504639 0.250162333 -78.43713379 0.252866775 -74.13915253 0.251965284 -69.84124756 0.253768265 -65.54333496 0.252866775 -61.24542236 0.253768265 -56.94750595 0.252866775 -52.64953613 0.252416044 -48.35162354 0.252416044 -44.05371094 0.252866775 -39.75579834 0.251514554 -35.45788574 0.253768265 -31.15991211 0.251514554 -26.86199951 0.251965284 -22.56408501 0.254669756 -18.26617432 0.251965284 -13.96826172 0.252866775 -9.670288086 0.252866775 -5.372375488 0.251514554 -1.074462891 0.252866775 3.223449707 0.253317535 7.521362305 0.251514554 11.81933594 0.252416044 16.11724854 0.251063824 20.41515923 0.251514554 24.71307373 0.250613064 29.01098633 0.253317535 33.30895996 0.251063824 37.60687256 0.251965284 41.90478516 0.251965284 46.20269775 0.252416044 50.50061035 0.252416044 54.7985878 0.252416044 59.09649658 0.252866775 63.39440918 0.252416044 67.69232178 0.253317535 71.99023438 0.251514554 76.28814697 0.252866775 80.58612061 0.252866775 84.8840332 0.252866775 89.1819458 0.252866775 93.4798584 0.251514554 97.777771 0.252866775 102.0757446 0.251965284 106.3736572 0.251965284 110.6715698 0.251965284 114.9694824 0.251965284 119.267395 0.254219025 123.5653687 0.252416044 127.8632813 0.253317535 132.1612549 0.251514554 136.4591064 0.252416044 140.7570801 0.251514554 145.0549316 0.250162333 149.3529053 0.251965284 153.6508789 0.253317535 157.9487305 0.252866775 162.2467041 0.252416044 166.5445557 0.250613064 170.8425293 0.254219025 175.1403809 0.253317535 179.4383545 0.253768265 183.7363281 0.252416044 188.0341949 0.252416044 192.3321533 0.252866775 196.6300049 0.252866775 200.9279785 0.252866775 205.2259521 0.251063824 209.5238037 0.252416044 213.8217773 0.251965284 218.1196289 0.251965284 222.4176025 0.251965284 226.7155762 0.251965284 231.0134277 0.250613064 235.3114014 0.250613064 239.6092529 0.251514554 243.9072113 0.251063824 248.2052002 0.250613064 252.5030518 0.253317535 256.8010254 0.252866775 261.098877 0.251965284 265.3968506 0.251965284 269.6948242 0.250613064 273.9926758 0.253768265 278.2906494 0.251965284 282.588501 0.251965284 286.8864746 0.253317535 291.1844482 0.252866775 295.4822998 0.253768265 299.7802734 0.252416044 295.4822998 0.248810112 291.1844482 0.249260843 286.8864746 0.250162333 282.588501 0.249260843 278.2906494 0.247908592 273.9926758 0.249260843 269.6948242 0.248359352 265.3968506 0.248359352 261.098877 0.248359352 256.8010254 0.248359352 252.5030518 0.247908592 248.2052002 0.248359352 243.9072113 0.248359352 239.6092529 0.249260843 235.3114014 0.249260843 231.0134277 0.247457862 226.7155762 0.246556371 222.4176025 0.247908592 218.1196289 0.246105641 213.8217773 0.247007132 209.5238037 0.247007132 205.2259521 0.246556371 200.9279785 0.248359352 196.6300049 0.246105641 192.3321533 0.247457862 188.0341949 0.247457862 183.7363281 0.247457862 179.4383545 0.249260843 175.1403809 0.248359352 170.8425293 0.248810112 166.5445557 0.248359352 162.2467041 0.245654896 157.9487305 0.246556371 153.6508789 0.247908592 149.3529053 0.248359352 145.0549316 0.247457862 140.7570801 0.248810112 136.4591064 0.247457862 132.1612549 0.247457862 127.8632813 0.246556371 123.5653687 0.246556371 119.267395 0.247457862 114.9694824 0.246556371 110.6715698 0.248810112 106.3736572 0.247007132 102.0757446 0.249260843 97.777771 0.246556371 93.4798584 0.247007132 89.1819458 0.247457862 84.8840332 0.246556371 80.58612061 0.247457862 76.28814697 0.246556371 71.99023438 0.247457862 67.69232178 0.248359352 63.39440918 0.247007132 59.09649658 0.247908592 54.7985878 0.247457862 50.50061035 0.248359352 46.20269775 0.248359352 41.90478516 0.246556371 37.60687256 0.246556371 33.30895996 0.247457862 29.01098633 0.247007132 24.71307373 0.247457862 20.41515923 0.247908592 16.11724854 0.246556371 11.81933594 0.248359352 7.521362305 0.247007132 3.223449707 0.247007132 -1.074462891 0.247908592 -5.372375488 0.247457862 -9.670288086 0.246556371 -13.96826172 0.247457862 -18.26617432 0.247457862 -22.56408501 0.246556371 -26.86199951 0.247457862 -31.15991211 0.246105641 -35.45788574 0.247457862 -39.75579834 0.247457862 -44.05371094 0.246556371 -48.35162354 0.248810112 -52.64953613 0.247457862 -56.94750595 0.247007132 -61.24542236 0.247457862 -65.54333496 0.248810112 -69.84124756 0.246556371 -74.13915253 0.247457862 -78.43713379 0.247908592 -82.73504639 0.247908592 -87.03295898 0.247007132 -91.33087158 0.248359352 -95.62878418 0.247457862 -99.92675781 0.248359352 -104.2246704 0.246105641 -108.522583 0.247908592 -112.8204956 0.246556371 -117.1184082 0.248359352 -121.4163208 0.248359352 -125.7142944 0.245204136 -130.012207 0.247457862 -134.3101196 0.246556371 -138.6080322 0.247457862 -142.9059448 0.247007132 -147.2039185 0.246556371 -151.5018311 0.247457862 -155.7997437 0.247457862 -160.0976563 0.247007132 -164.3955688 0.247007132 -169.2307739 0.247457862 -173.5286865 0.246556371 -177.8265991 0.248359352 -182.1245117 0.246105641 -186.4224854 0.247457862 -190.7203979 0.247457862 -195.0183105 0.247908592 -199.3162231 0.245654896 -203.6141357 0.245654896 -207.9121094 0.247457862 -212.210022 0.245654896 -216.5079346 0.247457862 -220.8058472 0.247007132 -225.1037598 0.246556371 -229.4017334 0.246556371 -233.699646 0.247007132 -237.9975586 0.247007132 -242.2954712 0.247007132 -246.5933838 0.247457862 -250.8913574 0.247007132 -255.18927 0.247007132 -259.4871826 0.249260843 -263.7850952 0.247007132 -268.0830078 0.247457862 -272.3809204 0.246556371 -276.678894 0.245654896 -280.9768066 0.248359352 -285.2747192 0.246105641 -289.5726318 0.248359352 -293.8705444 0.247007132 -298.1685181 0.247007132 -302.4664307 0.247457862 -306.7643433 0.245654896 -311.0622559 0.248359352 -315.3601685 0.247908592 -319.6581421 0.248359352 -323.9560547 0.247908592 -328.2539673 0.246556371 -332.5518799 0.246105641 -336.8497925 0.246105641 -341.1477661 0.245204136 -345.4456787 0.247457862 -349.7435913 0.246105641 -354.0415039 0.247007132 -358.3394165 0.247457862 -362.6373901 0.247007132 -366.9353027 0.247457862 -371.2332153 0.246556371 -375.5311279 0.247007132 -379.8290405 0.246556371 -384.1270142 0.246556371 -388.4249268 0.247457862 -392.7228394 0.248359352 -397.020752 0.248359352 -401.3186951 0.247908592 -405.6166077 0.247908592 -409.9145203 0.248359352 -414.2124634 0.247908592 -418.510376 0.247457862 -422.8083191 0.247908592 -427.1062317 0.246556371 -431.4041443 0.247457862 -435.7020874 0.246105641 -440 0.247007132 -444.2979431 0.247908592 -448.5958557 0.246105641 -452.8937683 0.247007132 -457.1917114 0.247908592 -461.489624 0.247457862 -465.7875671 0.246556371 -470.0854797 0.247007132 -474.3833923 0.246556371 -478.6813354 0.247457862 -482.979248 0.247908592 -487.2771606 0.247007132 -491.5751038 0.246556371 -495.8730164 0.248810112 -500.1709595 0.246105641 -504.4688721 0.246556371 -508.7667847 0.247908592 -513.0646973 0.247908592 -517.3626709 0.247457862 -521.6605835 0.246556371 -525.9584961 0.248359352 -530.2564087 0.248359352 -534.5543213 0.247007132 -538.8522949 0.247457862 -543.1502075 0.246556371 -547.4481201 0.247457862 -551.7460327 0.247457862 -556.0439453 0.246105641 -560.3419189 0.247457862 -564.6398315 0.246556371 -568.9377441 0.247007132 -573.2357178 0.248359352 -577.5335693 0.247457862 -581.831543 0.246105641 -586.1293945 0.246556371 -590.4273682 0.247457862 -594.7252197 0.246556371 -599.0231934 0.247908592 -603.321167 0.247007132 -607.6190186 0.247007132 -611.9169922 0.247908592 -616.2149048 0.245654896 -620.5128174 0.246105641 -624.810791 0.247007132 -629.1086426 0.247457862 -633.4066162 0.247908592 -637.7045288 0.246556371 -642.0024414 0.248359352 -646.300415 0.247007132 -650.5983276 0.247908592 -654.8962402 0.247457862 -659.1941528 0.247457862 -663.4920654 0.245654896 -667.7900391 0.247457862 -672.0879517 0.247457862 -676.3858643 0.248359352 -680.6837769 0.246556371 -684.9816895 0.248359352 -689.2796631 0.245204136 -693.5775146 0.247908592 -697.8754883 0.247007132 -702.1734009 0.246105641 -706.4713135 0.248810112 -710.7692871 0.247457862 -715.0671387 0.247457862 -719.3651123 0.247457862 -723.6630249 0.248359352 -727.9609375 0.247457862 -732.2589111 0.246556371 -736.5567627 0.248359352 -740.8547363 0.246556371 -745.1526489 0.245654896 -749.4505615 0.245654896 -753.7484741 0.247457862 -758.0463867 0.248359352 -762.3443604 0.245204136 -766.6422729 0.247457862 -770.9401855 0.247908592 -775.2380981 0.248810112 -779.5360107 0.246105641 -783.8339844 0.246556371 -788.131897 0.246105641 -792.4298096 0.246556371 -796.7277222 0.246556371 -801.0256348 0.247457862 -805.3236084 0.247457862 -809.621521 0.248359352 -813.9194336 0.246105641 -818.2173462 0.248359352 -822.5152588 0.246105641 -826.8132324 0.247457862 -831.111145 0.246556371 -835.4090576 0.246556371 -839.7069702 0.247007132 -844.0048828 0.246556371 -848.3028564 0.245204136 -852.600769 0.248359352 -856.8986816 0.247007132 -861.1966553 0.247007132 -865.4945068 0.247457862 -869.7924805 0.246556371 -874.0903931 0.246105641 -878.3883057 0.248359352 -882.6861572 0.246556371 -886.9841309 0.246105641 -891.2821045 0.247007132 -895.5800171 0.246556371 -899.8779297 0.247908592 -895.5800171 0.249260843 -891.2821045 0.251514554
Stimulus varies from -900mV to 300mV.
Random load:

Yes, I am using that one only.
You may check VCE-VSE voltage as that is the stimulus voltage.
Can you please tell me, how did you got stimulus voltage?
I exported the excel data from Sensorpal GUI.
Okay...In my case, I am using Aducm355qspz which don't supports Sensorpal GUI..
You may capture VCE-VSE voltage on oscilloscope.
By using Realterm only...