Hello, I want to know how much maximum voltage can be applied across AIN0+ & AIN0-, if AVDD is 3.3 V, VREF is 2.5 V.
AD7770
Recommended for New Designs
The AD7770 is an 8-channel, simultaneous sampling ADC. Eight
full sigma-delta (Σ-Δ) ADCs are on chip. The AD7770 provides
a low input current to allow...
Datasheet
AD7770 on Analog.com
Hello, I want to know how much maximum voltage can be applied across AIN0+ & AIN0-, if AVDD is 3.3 V, VREF is 2.5 V.
Hi Rranjan ,
Please refer to the FAQ below that discusses the maximum voltage for different input configurations - differential, pseudo differential, or single ended.
Thanks,
Janine
But maximum voltage limit across analog input pin respect to what? It's not clear, please explain is it with respect to AGND or AIN-?
Hi Rranjan ,
The limits of the AINx+ pin with respect to AINx- (differential analog input) is limited by the "Differential Input Voltage Range" below and depends on the reference voltage.
While the limit of the analog input pins (AINx+, AINx-) with respect to ground is the "Absolute AINx+- Voltage Limits" below and depends on the Analog supplies.

The excel file combines the limitation provided by the reference input and analog supplies to state the analog input limits conforming to both.
Thanks,
Janine
Hi JEstayo,
Is it necessary to integrate AD7770 with any OP-AMP to get better accuracy? If yes, could you please suggest with any application circuit for AD7770.
Hi JEstayo
I am asking for better accuracy or precision, or there would be any design issue if I don't use any OPAMP with this.
Thanks,
Ravi