Post Go back to editing

AD7329 Spi Problem

Category: Hardware
Product Number: AD7329
Hi, we use Ad7329 ADC in our custom board. We work with NXP S32K344 MCU. When I try to read measurement result, I always read different meaningless values. At the below, I attached scope pictures, schematic and configurations of SPI interface. Can you help me to figure out to problem?
 
AD7329 Schematic
SPI Configuration:
 
 
Use Senario: 3.3V Vcc 0-10 V single ended, no sequence, only read channel 1 for test
 
 
Range Register BFE0
(Green: Miso
Yellow Mosi
Red CS
Blue Clk)
 
Seq Reg E800
 
Control Reg 8632
 
Read Command  and Result (0000)
 
 
It give me always different meaningless result. I can not read true value. In test, I gave it 2.66 V but result is not even close. Can you help me?